In order to meet these requirements, great importance is placed on suitable suppliers: "We employed plain bearings from igus in all the motion areas of the hydraulic cylinder." This collaboration has proven its worth for more than ten years. Orders are with us within half a week. " The installed "iglidur G" products are also beneficial with short delivery times as well as technical advantages. They are significantly more economical compared to the brass bushings used earlier. In addition, the bearings, which are used with diameters of 20 to 45 millimetres, are extremely wear-resistant and weather-resistant.
The robustness of the bearings is very important for Wichert: "As our customers are based in Southern Germany, Switzerland and Dubai, the prevailing temperatures can fluctuate between -15°C and +70°C. Added to this is the salt content in the air during the winter periods. We can't afford any downtime here. " Uwe Sund, igus industrial manager for agricultural engineering, confirms these experiences: "Plain bearings made of iglidur G cover the widest range of different requirements. The material is ideal for universal applications, a truly "all-round". Typical applications include medium to high loads, medium surface speeds and medium temperatures. “
Hétfotol péntekig reggel 7 és este 8 között.Szombaton reggel 8 és 12 között.
24h