Az ország/régió kiválasztása befolyásolhatja az árat, a szállítási lehetőségeket és a termékválasztékot.
Média |
|
Van kérdése? Anyagra van szüksége? Aktuális sajtóinformáció és publikálásra kész fotóanyag letöltésre elérheto itt. Emellett telefonon, e-mailben és faxon is érdeklodhet. |
|
Press contactSzeretne felkerülni a média terjesztési listánkra? |
Drive cable delivered fast after easy online search and order2018.11.27.
If the user is looking for a highly flexible drive cable, then igus offers technically the best and the most cost-effective solution from more than 4200 cable types according to 24 manufacturer standards with the readycable product finder. Simply enter the part number of igus or the manufacturer, or select the name of the drive manufacturer from the menu. Then click on the required cable type and the product finder will list all suitable drive cables. The overview covers the various cable qualities, such as PUR, PVC or TPE outer jacket, including their most important properties such as bend radius and travel length. The newly integrated service life calculator predicts the lifetime of the cable in the e-chain after entering various parameters, such as speed, operating temperature and acceleration. The price is also displayed. With another click, the selected part can be added to the shopping cart. The chosen drive cable is delivered to the required length, with centimetre accuracy, and shipping starts from 24 hours. All this without surcharges, and from a quantity of one. |